5G Means Data Center Platforms Must Evolve
Image Source:
buffaloboy/Shutterstock.com
By Alex Pluemer for Mouser Electronics
Published January 18, 2021
5G is the next frontier of cellular connectivity, but the new generation promises more than just faster download
speeds and lower latency. The higher bandwidth and more comprehensive coverage 5G is expected to deliver will
open up various new use cases for connectivity beyond just cellular phones, ranging from laptops and handheld
Internet of Things (IoT) devices to automobiles and large-scale industrial implementations. Industry forecasts
predict that 5G will gain over 1 billion subscribers by the mid-2020s as the migration from 4G devices that
aren’t compatible with 5G networks takes place. However, transitioning to 5G will require a major
investment in new cellular infrastructure. 5G architecture will change substantially from preceding
implementations. Driving these changes are some of the key characteristics of 5G that have evolved from the
fourth generation. We’ll review these key characteristics and then see how these will affect the data
platform architecture for a typical 5G system, and explore the implementation options for various levels of data
platforms and identify typical implementation options. We’ll also look at an example mid-range data
platform in detail to identify key design choices and trade-offs.
5G Characteristics Drive Implementation Architecture
Low-band 5G cell towers operate on a frequency range similar to 4G cellphones (from 600MHz to 850MHz and provide
similar range and download speeds (30Mbit/s to 250Mbit/s). As a result, low-band 5G is already being phased out
in many areas of the world. Mid-band 5G towers employ microwaves of between approximately 2.5GHz and 3.7GHz,
significantly increasing download speeds to the 100Mbit/s-900Mbit/s range while expanding coverage range by
several miles. Mid-band 5G towers are already the norm in big cities and other high-population areas and could
soon become the worldwide standard.
High-band 5G currently operates in the 25GHz-39GHz range and delivers download speeds similar to cable internet
service, which is about 1Gbps. High-band 5G does have limitations, however. Operating at the 25GHz-39GHz range
is on the low end of the millimeter-wave (mmW) band. mmW has a more limited range than microwaves, meaning
high-band 5G will require a greater number of smaller cells to cover the same area as mid-band 5G. Physical
obstructions such as walls or home appliances can also limit high-band 5G connectivity. mmWs also don’t
negotiate solid objects well. High-band 5G is also much more costly than lower-frequency technology. As a
result, high-band 5G might be limited to large, relatively open facilities such as concert venues and sports
arenas in the near future.
The Pyramid of 5G Data Platforms
Factors such as coverage range, required download speed and cost efficiency have to be considered when
determining the 5G hierarchy level for a specific implementation. The 5G distributed data platform places data
processing, storage, and communications at various levels of the architecture hierarchy to optimize cost, power,
network performance, operating distance, and user features. Closest to the network’s edge are small
pico-platforms that cover small distances (tens of meters) within a building or facility. Common examples
include building automation, security, factory floor module monitoring, and control. On the level above edge
devices are aggregation platforms that stitch together all the edge devices and consolidate and optimize data
traffic over a distance of approximately 100M. These devices are often located at the building or small campus
level and can analyze, filter, combine and prioritize communications, sometimes with artificial intelligence
(AI) cooperation.
Intermediate platforms are positioned on the level below massive central data centers (core) to deliver quicker
responses. These responses are often algorithm-based selected by and periodically updated from the core. These
platforms provide the real-time control needed for the platforms closer to the edge. Data analysis and tracking
from these platforms can provide value and new income streams to the platform providers. Cost savings from
operations such as predictive maintenance, material tracking and routing, system management, and data traffic
load balancing can be passed on to the user (perhaps for a subscription fee or percentage of the savings).
Big data operations are run on core data-center platforms. These massive data processing and storage facilities
hold years’ worth of historical operations and complex machine-learning algorithms that provide the
optimization filters and processes to program intermediate platforms for quick responses─and added value to
customers.
Evaluating Different Types of Data Center Platforms
At each level of the 5G hierarchy, different requirements and trade-offs are presented to the designer:
- Small platforms are the most cost-, footprint- and power-constrained elements of the system. They need to be
easy to install and require a mid-range lifetime because several are needed for each aggregation platform.
MCU-based implementations can be used here since they provide the low cost, low power, and small footprint
required while making some minor sacrifices regarding flexibility and processing power.
- Aggregation platforms require significant flexibility, processing power, intermediate storage, and security.
Field-programmable gate array-based implementations can provide a maximum amount of flexibility and
processing power since the underlying hardware can be reprogrammed as needed for new protocols, new AI
algorithms, or new value adds to customers. FPGAs can also be easily scaled, allowing providers to create
different product tiers with varying flexibility and processing power levels at different price and value
points.
- Intermediate platforms require the highest level of raw processing power, security, and flexibility. Cost,
power consumption, and footprint are acceptable sacrifices. At this level, a hybrid combination of memory
protection units (for raw processing power of common operations) and FPGAs (for flexibility and
adaptability) will be the optimal implementation approach. The FPGA can even be reprogrammed in real time on
an as-needed basis to respond to the increased need for important features such as video processing,
encryption, decryption, searching, and filtering. AI algorithms can even predict such needs by analyzing
clues they find in key metrics such as occupancy, traffic patterns, weather, etc.
How an Aggregation Platform Works
Let’s take a look at a mid-range featured aggregation platform to see how key features are implemented
within the device. Utilizing an FPGA with an on-chip microcontroller allows the device to begin operation from
the MCU, providing a known secure starting point for boot and secure updates. This root of trust uses robust and
protected encryption, decryption, and security key storage operations to thwart hackers and viruses from taking
over the system. The MCU can also handle standard operations such as communications, packet processing, video
processing, compression, and storage efficiency. The on-chip FPGA hardware can be used for the less common but
processing-power-intensive operations to keep the MCU freed up for common operations that must be completed in a
timely manner.
The FPGA can be used for digital filtering, image processing, image recognition, and similar special operations,
perhaps in conjunction with AI and machine-learning algorithms to predict and program the hardware on an
as-needed basis. Over time, new algorithms could be identified, created and downloaded from intermediate and
core platforms to further optimize performance and to create new revenue streams for the platform provider─and
cost savings for the customer.
Conclusion
5G will mean bringing together cloud, core and the edge. However, it’s important that each of these runs
on─or has access to─the right types of infrastructure. A core will always be needed, even with the importance of
edge computing for 5G, but as 5G connectivity proliferates and the number of 5G-enabled devices continues to
grow, so will the need for small and intermediate distributed data center platforms for those devices. Computing
from the core all the way down to the edge will be the hallmark of the 5G-enabled world. It will be a world in
which thermostats and refrigerators to planes, trains and automobiles are connected to the same cellular network
as cell phones.
Author Bio
Alex is a senior technical writer for
Wavefront Marketing specializing in advanced electronics, emerging technologies and responsible technology
development.