Threat Models Identify Design Exposures
Image Source:
andreiodo/Shutterstock.com
By Stephen Evanczuk for Mouser Electronics
Edited November 23, 2020 (Originally Published May 30, 2019)
In combining peripheral sensors, gateways, and cloud resources, Internet of Things (IoT) applications are
becoming unprecedented targets because of the number of potential attack surfaces and security vulnerabilities
they contain. A clear understanding of such threats, their likelihood, and impact becomes more urgent as
enterprises tie these applications more tightly into corporate infrastructures. Using methodical approaches to
threat and risk assessments, development teams can harden security where essential or make informed decisions
about acceptable risks.
The wide range of security vulnerabilities in connected systems finds expression all too frequently in news
reports. A quick dip into the headlines shows a startling breadth of attacks, ranging from overt, massive
distributed denial-of-service (DDoS) attacks to extremely covert advanced persistent threats (APTs) that linger
and quietly extract valuable data or prepare for more extreme strikes.
Despite the sensationalist nature of these exploits, one of the most important lessons learned from these attacks
is that the use of security mechanisms and the creation of a secure system are not the same. Hackers
successfully penetrate systems that are built with all manner of security mechanisms. Even the most
security-conscious development team can unknowingly leave open attack surfaces in their designs.
The sheer complexity of today's designs increases the chance of open attack surfaces, particularly with
multilayered, connected systems such as IoT applications. When large numbers of programmable devices of
different types connect to the cloud, end-to-end security becomes more of a statistical probability than an
absolute certainty. Each element in such an interconnected system of systems contributes its specific
functionality and its own set of vulnerabilities to the security equation. By fully understanding how each
vulnerability can become a threat to the overall application, an enterprise can decide whether the associated
risk of a successful exploit of that vulnerability will rise above the threshold of acceptance and ultimately
require mitigation.
The ability to gain this level of visibility into the nature of a risk provides strategic value that cannot be
overstated. At the same time, by intersecting security vulnerabilities with risk assessments, a development team
can devise a tactical roadmap for developing a practical response to the nearly endless stream of threats to any
connected system. Indeed, without a more rigorous level of understanding gained through threat and risk
assessments, even the most experienced development team is gambling on the security of their systems and
applications. However, gaining this knowledge starts with a clear understanding of the potential threats against
a system, which is achievable through a well-documented threat model.
Threat models capture the specific security vulnerabilities associated with a system’s design. Creating a
threat model seems simple conceptually: Developers analyze their designs to identify security vulnerabilities
that relate to each underlying component. However, in practice, threat modeling can involve much more work,
research, and strategy than this simple idea suggests—and can yield far more than a list of technical
security concerns. More broadly applied, threat modeling can also identify vulnerabilities in the associated
life-cycle processes and overarching security policies that correlate with an IoT application. Ultimately, what
constitutes acceptable threat models can vary as widely as the IoT applications and organizations they serve.
Different threat models share certain characteristics, and any threat modeling methodology will follow a few
common steps. Let’s examine them.
Threat Modeling
Threat modeling begins with an accurate description of the system, the so-called Target of Evaluation (TOE),
associated with a specific use case, such as the utility water-meter’s operation. If a threat model paints
a picture of system vulnerabilities, the TOE description is the canvas. By widening or tightening the
TOE’s scope, a threat modeling team can expand or contract the focus in a threat identification process.
For example, Arm’s recently released smart water-meter threat model sharply restricts its TOE, focusing
only on the system's core (Figure 1).
Figure 1: Arm's water-meter threat model limits its TOE to the system’s core
rather than including the full complement of subsystems typically included in these systems, resulting in a
more manageable scope of analysis. (Source: Arm)
Of course, a TOE confined within a single subset of a larger, more complex system or application translates to a
more limited ability to identify threats, assess risks, and build an effective mitigation plan. For a complex
system of systems such as an IoT application, experienced threat modelers might create a series of threat
models, going from a fairly abstract description of the complete system to increasingly detailed descriptions of
subsystems of particular importance or concern to the organization.
Whatever the approach, no absolute requirement for the level of detail is required in the TOE description.
Modeling approaches that intend to provide each component’s exhaustive details can simply exhaust the
participants in the process. On the other hand, models that are too abstract are likely to hide subtle
vulnerabilities or prevent the identification of vulnerabilities buried deeply in a chain of dependencies or
third-party software libraries.
An effective middle ground collects an evolving level of detail up to the necessary level to capture all
interactions that cross trust boundaries between the system’s separate, unique zones (Figure
2). For example, an IoT application can comprise multiple zones linked with cloud resources,
gateways, IoT terminal devices, and users. Transactions that operate across trust boundaries are particularly
vulnerable to an exceptional array of attacks on transferred data, security credentials, or protocols. Even
seemingly innocuous attempts to communicate across a trust boundary can create a pathway for a fingerprinting
attack—where hackers use known indicators in the system’s response to determine the system’s
underlying components in preparation for more directed attacks.
Figure 2: Threat models should provide sufficient details to identify
possible transactions that cross trust boundaries between different system zones. (Source: Microsoft)
Of course, understanding the interactions between the underlying components within each zone becomes especially
important if some of those components come from third parties. For example, an IoT device that uses a
third-party sensor driver could be vulnerable to threats at the driver’s boundary (Figure
3).
Figure 3: Although this data-flow diagram was designed to illustrate
transactions that cross the boundaries of desktop software drivers, the same principles apply to
transactions involving third-party hardware or software components in any connected system, including IoT
devices. (Source: Microsoft)
Although a suitably detailed description is essential for threat modeling, identifying specific threats that
connect to those details is the payoff. In the case of Arm’s water-meter threat model, the modelers
provide a plain-language list of threats associated with each asset, such as firmware, measurement data, and
interactions with external entities (such as users, administrators, and attackers), that might touch the TOE.
For firmware, the model describes specific threats, including the installation of compromised firmware,
modifications of associated security certificates utilized to authenticate firmware updates, cloning, and more.
Based on the list of assets and identified vulnerabilities, development teams can evolve corresponding security
objectives and mitigation methods. For example, Arm’s water-meter model concludes with a list of security
requirements, including those for firmware, such as the need for a secure boot, firmware authentication, a
response to a failed authentication, and others.
Available Resources
In identifying potential threats, few (if any) development organizations can remain current on every possible
threat that might apply to the detailed assets and processes included in their TOE descriptions. The good news
is that engineers can find several published sources to help with this part of the process. Developers can use
public resources such as the Common Attack Pattern Enumeration and Classification (CAPEC) list to review, from
the top down, the most likely types of attacks. Then, they can work, from the bottom up, to identify the likely
targets of attack listed in the Common Weakness Enumeration (CWE) list, which describes inherent flaws in system
design approaches, such as using hardcoded credentials. As designers identify specific hardware or software
components utilized in their designs, they can turn to the Common Vulnerabilities and Exposures (CVE) list,
which lists specific software flaws or potential exploits in available hardware or software components.
For risk assessments, resources such as the Common Vulnerability Scoring System (CVSS) provide a consistent
approach for rating the risks associated with specific vulnerabilities. Although a risk relates to the nature of
a specific vulnerability, it also includes other factors such as the avenue (vector) used to perform the attack,
the complexity of the attack required to exploit the vulnerability, and others. For example, an attack that can
be performed through a network brings considerably more risk than one that requires physical access. Similarly,
an attack that is simple to perform carries significantly more risk than a highly complex attack. Using a CVSS
calculator, engineers can quickly account for these various contributing factors, arriving at a numeric score
for the risk level associated with a particular threat or class of threats. For Arm’s water meter, the
CVSS calculator finds that the combination of factors involved in a firmware attack represents a critical risk
score of 9.0 (Figure 4).
Figure 4: Using the CVSS calculator, development teams can assign specific
risk levels that correlate with different vulnerabilities for TOE assets, such as the firmware in Arm’s
water-meter threat model. (Source: FIRST.org)
Because of the broad range of requirements and techniques, automated tools such as Open Web Application Security
Project’s (OWASP’s) Threat Dragon Project, Mozilla's SeaSponge, and Microsoft's Threat Modeling Tool
exist to help developers work through the modeling process. Each uses a different threat modeling methodology,
ranging from system diagramming in the Threat Dragon Project and SeaSponge to Microsoft's detailed STRIDE
(translated as Spoofing, Tampering, Repudiation, Information disclosure, Denial of service, and Elevation of
privilege) approach. Although these tools are several years old and generally built for enterprise software
systems, threat modeling is a broadly applicable, evergreen process that depends more on the current lists of
attack vectors, weaknesses, and vulnerabilities than on specific methodologies. Nevertheless, newer tools are
emerging that promise a tighter link between a system description and threat identification. Despite the rapid
emergence of deep-learning technologies in other areas, significant challenges remain in applying these
technologies to automated threat and risk assessments. Even so, the availability of smart modeling and
assessment tools is likely soon to come.
In the meantime, developers can find various collections that list security weaknesses, vulnerabilities, and
attack patterns—so much so that all the available detail can seem overwhelming, particularly to those just
starting to engage in threat modeling. One of the excuses commonly used to avoid threat modeling is that it is
simply too complicated. Rather than jumping into the full depth of details, engineers can start with a more
modest approach that focuses just on the most common threats. OWASP’s list of top-10 IoT security threats
provides a useful starting point. Developers need to go no further than their preferred news sites to find a
ready catalog of top vulnerabilities and exploits.
For organizations able to move quickly past the basics, however, these same methods can prove invaluable in
addressing equally critical aspects of IoT design. For example, systems used in machine-control loops typically
face associated mission-critical requirements for functional safety. In these systems, security and functional
safety are so intertwined that suitable threat models for these systems will likely need to include scenarios
where security or safety weaknesses can equally lead to physical risks. In the same way, security and privacy
overlap in many respects, yet weaknesses in either area can lead to a disclosure of personally identifiable
information.
Conclusion
The effective application of threat modeling and risk assessments in complex systems goes well beyond any simple
list of available options and techniques. Like each specific system, each development organization deals with
its own unique constraints and capabilities. The requirements for one system or organization might completely
miss the mark for another. What might be the only common requirement is the need to perform threat and risk
assessments in the first place. Even so, should an enterprise attempt to create a complete threat model and risk
assessment? The short answer is no. An attempt to do so would fall short of this perfect objective.
It is not possible to perfectly predict outcomes. Naturally, the world’s chaotic processes and the ebb and
flow between system mitigations and hacker exploits ultimately derail any attempts toward perfection. At the
same time, without building the kind of security roadmap that a threat model and risk assessment provide, it is
equally impossible to avoid at least some of the pitfalls and detours that lead to inevitable security breaches.
Stephen Evanczuk has more than 20 years of
experience writing for and about the electronics industry on a wide range of topics including hardware,
software, systems, and applications including the IoT. He received his Ph.D. in neuroscience on neuronal
networks and worked in the aerospace industry on massively distributed secure systems and algorithm acceleration
methods. Currently, when he's not writing articles on technology and engineering, he's working on applications
of deep learning to recognition and recommendation systems.