Driver Design in Piezoelectric Motors
By Bill Schweber for Mouser Electronics
For most electrical engineers, the simple term “motor” means
one thing: An electromagnetic rotary-motion unit. Engineers who need linear rather than rotary motion consider
adding a mechanical linkage of some sort or perhaps a linear-induction electromagnetic motor. However, the
conventional electromagnetic motor—whether rotary or linear, or large or small—is often not the best
choice for precise, minute linear motion because of challenges in control, mechanical tolerances, backlash, and
other electrical and mechanical issues. Fortunately, there is a very viable alternative: The piezoelectric motor,
which is used extensively in a wide variety of applications that need precise control of tiny ranges of linear
motion.
Piezoelectric Motor Overview
This fascinating, unconventional motor is based on the well-known and widely-used piezoelectric effect, which is a
symmetrical electrical-mechanical relationship. Under this effect, when a crystal material is subject to mechanical
stress (squeezed), it generates a voltage; when a voltage is applied to the same crystal, the material expands by a
very small amount. This pair of piezoelectric properties has been exploited with great success in the classic
crystal-based oscillator, which has formed the basis of a clock/frequency source for nearly 100 years (although
MEMS-based oscillators are coming on strong as an alternative in recent years).
In the piezoelectric motor, an electric field is applied to the crystal material (via a voltage across the
material) and the material elongates very slightly, on the order of 0.01 to 0.1 percent for typically-applied
voltages. These motors are small (one of their many virtues) with a representative device being about 10mm in each
dimension (larger ones are also in use), and the resultant motion on the order of microns, yet with Newtons of
force. Larger elongations with more force can be achieved by stacking and driving multiple piezoelectric crystals as
a single unit.
This physical elongation can be employed in two ways. In one arrangement, the piezo material can alternately be
held and then released by a set of tiny piezo-based clamps, thus allowing the crystal to inch forward (appropriately
called inchworm mode), as shown in Figure 1.
Figure 1: With appropriate timing of clamping and unclamping with respect to
piezo-motor actuation, the motor can move ahead in tiny increments similar to an inchworm (1-housing, 2-moving
crystal, 3-locking crystal, 4-rotary part). (Source: Laurensva Lieshour / CC BY-SA 3.0)
Alternatively, one end of the crystal can be clamped in place while allowing the other end to move back and forth
as the voltage is applied and removed, resulting in a piston or slip-stick motion (Figure 2). An
array of multiple piezo motors can also be arranged in a circle to provide rotary motion, although their primary use
is linear motion.
Figure 2: With one end fixed in place, the piezo motor becomes a precise,
highly-controllable piston. (Source: Inductiveload / CC BY 2.5)
Piezo-based motion is used in infusion pumps, microscope stages, optical positioning, instrumentation, inkjet
nozzles, and more; inexpensive, lower-quality piezo devices are used for audio sounders, alarms, and even small
loudspeakers, but those uses have relaxed performance requirements. Piezo motors can be fast, can reach into the
multi-kHz range—impossible with electromagnetic motors—and are precise, repeatable, and controllable.
Further, they are clean, with no bearings needing lubricant that may cause contamination, while their non-metallic
nature is also an advantage in many situations (and may even be a necessity, as in MRI machines).
Drivers Make the Difference
As with electromagnetic motors, a complete and useable piezo-motor assembly consists of three parts: The electronic
drive, the electrical-mechanical transducer (motor) itself, and the output linkage. We’ll be focusing on the
drive electronics.
For electromagnetic motors, the drive function requires sourcing and sinking current into the electromagnetic
coils, which is usually done using power semiconductors (MOSFETs or IGBTs). These power devices are controlled by
drivers that turn them on and off at the correct times, with appropriate slew rates, and they must source/sink the
required current into their highly inductive loads. The voltage that is applied to the MOSFET or IGBT output stage
is needed to force the current into the coils, but it is the current that provides the electromagnetic force for the
motor coils.
For piezo motors, the situation is very different. Instead of driving current, the driver must supply a relatively
high voltage to create the electric field, and current is the secondary factor accompanying this applied voltage.
Thus, the piezo drive scenario is the complement of the electromagnetic drive, where current drive is needed and
voltage is a consequence; here, voltage is what is needed and current is the consequence. The piezo driver must
supply the needed voltage (not current) into a capacitive (not inductive) load, and it must control and modulate
this voltage to force the desired crystal elongation. In other words, current is the independent parameter and
voltage is the dependent parameter for conventional motors, but for piezo motors, the situation is the opposite.
The piezo motor’s needed voltage (and therefore current) levels depend on the size of the piezoelectric
element, the intended elongation, and the rate of motion. At the low end, voltage and current values may be
20–30V and 10–30mA, respectively, but most higher-performance piezo units need at least 10V and 10 to
several hundred milliamps, and there are even piezo motors using 1,000V and above at several amps.
It’s this need to provide high voltage at moderate currents that is the electrical design challenge. In
addition, the piezo driver must remain stable despite the highly-capacitive nature of the load, which can read
1,000pF (1nF) and more. Also, as the piezo device is a floating, differential device most applications require a
differential, bipolar driver output.
One major design caution: Since these motors operate at higher voltages, there are issues of user safety, physical
isolation and protection from the voltages, and regulatory mandates defining minimum creepage and clearance
dimensions, which are a function of the voltage level. Therefore, any driver circuit for a piezo motor must keep
these layout and placement conditions in mind, in addition to what works for the circuit’s electrical
performance. Also note that these high voltages and modest current pairings are not unique to piezo devices, as many
scientific and even commercial products need this combination, such a neon lights, special vacuum tubes,
electrometers, and optical equipment, to cite a few.
Driver Design Offers Options
Developing and delivering the relatively-high voltages needed for piezo drivers is a challenge in many cases
because most amplifier ICs are low-voltage devices, while the higher-voltage ones are usually optimized for the
current drive needed by MOSFETs/IGBTs, rather than for voltage drive. There are some specialized operational
amplifiers (op amps) that are designed for piezo drive at the higher currents and voltages using high-voltage IC
processes or for hybrid devices that combine lower-voltage op amps with voltage-boosting transistors on their
output.
In principle, it is possible to build a basic high-voltage driver using just a transistor with adequate voltage
rating (Figure 3). However, this design lacks the precision, controllability, and stability that a
higher-performance piezo driver needs, and it also lacks protection features for failure modes. Further, it is not
capable of delivering bipolar output, while its base-circuit drive requires suitable circuitry. Therefore, this type
of basic design is better suited for less technically-challenging applications such as piezo alarms and sounders.
Figure 3: While a piezo element can be controlled by a basic transistor, the
configuration is suitable only for modestly-challenging applications such as piezo-based speakers. (Source:
Murata)
Fortunately, vendors have developed ICs that are specifically designed for piezo drive and simplify the task while
adding needed features and functions, including control of the high-voltage waveform slew. These ICs also offer
thermal, overload, and short-circuit protection, which are must haves in practical designs.
From Analog Devices
For example, Analog Devices offers the ADA4700-1, a high-voltage precision amplifier with a wide
operating voltage range of (±5 to ±50V). Although this eight-lead SOIC device looks like a standard op
amp, it is optimized for providing high-slew rate output into capacitive loads while remaining stable,
Figure 4. It is fully characterized for a wide variety of operating conditions (at various
voltages, loads, temperatures, distortion levels, and overshoot, for example) and is supported by a data sheet that
features over 60 graphs of performance across many scenarios.
Figure 4: The ADA4700-1 high-voltage precision amplifier has carefully defined
slew rate performance, along with many other attributes that are fully detailed in the data sheet. (Source: Analog
Devices)
The ADA4700-1 is stable with minimal overshoot when driving capacitive loads, but extra compensation can enhance
the response when driving larger capacitances. This requires a small snubber network, Figure 5; for
unity-gain applications and capacitive loads up to 1nF (1,000pF), a combination of a 150Ω resistor and 10nF
capacitor are all that is needed. For larger loads up to 10nF and higher gains such as tenfold, the resistor is
decreased to 22Ω while the capacitor increases to 100nF. Finally, the drive-current level can be boosted by adding
an external pair of complementary (PNP/NPN) transistors (Figure 6).
Figure 5: For driving highly capacitive loads, a simple external RC snubber
circuit is added to the ADA4700-1. (Source: Analog Devices)
Figure 6: If additional output current is needed, a PNP/NPN transistor pair is
added to the output of the ADA4700-1. (Source: Analog Devices)
From Texas Instruments
Texas Instruments also offers devices that are well-suited to piezo-type loads.
Their DRV8662 piezo haptic driver with integrated boost converter
has a high degree of functionality, including a 105V boost switch (Figure 7), yet it requires just
a 3.0 to 5.5V supply. The boost voltage is set using two external resistors, while the device gain can be set to one
of four values using two I/O lines.
Figure 7: The DRV8662 is a piezo driver targeting haptic applications and
delivers over 100V from a single-digit supply. (Source: Texas Instruments)
It features a range of drive capability. For example, at 300Hz operation, it is specified to drive 100nF at
200VPP, 150nF at 150 VPP, 330nF at 100VPP, and 680nF at 50VPP. Despite
its internal complexity, this twenty-lead, 4 × 4mm QFN is simple to use, as shown by its interconnection
(Figure 8).
Figure 8: Despite its internal complexity, using the DRV8662 in a circuit
requires just a few external components to set basic operating parameters. (Source: Texas Instruments)
From Microchip
Some vendors of piezo-related ICs have gone beyond just providing ICs and their basic support documents such as
data sheets, and instead offer detailed reference designs. Microchip Technology, for
example, offers a complete design for a piezo-motor fluid micropump. The design includes a block diagram
(Figure 9), flow charts, code, schematic, and layout, and also shows the low-voltage
power-subsystem for the charger, microcontroller, and other components, plus the high-voltage section that drives
the piezo-based pump.
Figure 9: Going well beyond the data sheet, Microchip Technology has a
detailed application note providing a complete design, including software, for a fluid micropump controller driven
by a piezo motor. (Source: Microchip Technology)
The design uses a pair of ICs for its high-voltage section (Figure 10) and is capable of
delivering up to 250VPP at a maximum frequency of 300Hz. The design is based on the HV9150 DC/DC boost
converter working with the HV913 high-voltage driver. The boost converter transforms the low-voltage rail from the
rechargeable battery to 250V, which is then used to power the driver IC to actuate the piezoelectric micropump. The
driver IC provides a high-voltage, unipolar, push-pull output and a series of pulses are generated from the
controller IC to drive the piezoelectric element. The final design is not just a paper concept, but has been built
and tested (Figure 11).
Figure 10: In addition to the conventional low-voltage subsection, the design
uses a two-IC approach to boosting and managing the design’s low-voltage rail to the 250V level needed by
the piezo pump. (Source: Microchip Technology)
Figure 11: The piezo micropump controller is a built and tested unit, and the
application note provides numerous waveform details and test code. (Source: Microchip Technology)
Summary
Piezoelectric motors are an effective solution to many micro-motion applications, where minute linear motion along
with precision control is needed. They can replace electromagnetic rotary and linear motors, and in appropriate
applications they offer superior performance across many parameters along with some unique features that
conventional motors cannot provide. Due to their higher-voltage drive requirements (rather than current) and
capacitive loading (rather than inductive), their driver demands differ from electromagnetic motors.
Standard op amps can be used with appropriate external voltage-boost transistors to provide the combination of high
voltage and modest current. However, IC vendors offer devices that are optimized for driving piezo elements and
include extra features such as better control of the output drive, thermal and other shutdown-safety features,
short-circuit protection, and more, thus simplifying the design-in while enhancing performance.
Bill Schweber is a contributing writer for Mouser Electronics and an electronics
engineer who has written three textbooks on electronic communications systems, as well as hundreds of technical
articles, opinion columns, and product features. In past roles, he worked as a technical web-site manager for
multiple topic-specific sites for EE Times, as well as both the Executive Editor and Analog Editor at
EDN.
At Analog Devices, Inc. (a leading vendor of analog and mixed-signal ICs), Bill was in marketing communications
(public relations); as a result, he has been on both sides of the technical PR function, presenting company
products, stories, and messages to the media and also as the recipient of these.
Prior to the MarCom role at Analog, Bill was associate editor of their respected technical journal, and also
worked in their product marketing and applications engineering groups. Before those roles, Bill was at Instron
Corp., doing hands-on analog- and power-circuit design and systems integration for materials-testing machine
controls.
He has an MSEE (Univ. of Mass) and BSEE (Columbia Univ.), is a Registered Professional Engineer, and holds an
Advanced Class amateur radio license. Bill has also planned, written, and presented on-line courses on a variety
of engineering topics, including MOSFET basics, ADC selection, and driving LEDs.