Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

TI's LMZM3360x Power Modules, Now at Mouser, Integrate 36V Buck Converter and Power Circuitry in a Compact Package

May 21, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the LMZM33602 and LMZM33603 power modules from Texas Instruments (TI). These completely integrated 4 V-36 V power module solutions combine a step-down DC-to-DC converter with power MOSFETs, a shielded inductor, and passive components in a compact, low-profile package. To simplify design and offer even greater ease-of-use, the LMZM33602/LMZM33603 power modules require as few as four external components and enable engineers to eliminate the loop compensation and magnetics part selection from the design process.

The TI LMZM3360x power modules, available from Mouser Electronics, are 2 A (LMZM33602) or 3 A (LMZM33603) synchronous step-down DC-DC converters. The LMZM33602 offers an output voltage range from 1 V to 18 V at 2 A, whereas the output voltage range of the LMZM33603 is 1 V to 13.5 V at 3 A.. Both converters allow synchronization to an external clock and feature an adjustable switching frequency from 200 kHz to 1.2 MHz. The switching frequency can also be adjusted by either an external resistor or a sync signal, which allows the solution to accommodate a variety of input and output voltage conditions as well as optimize efficiency up to 95 percent.

For support and development, the LMZM3360x power modules utilize the LMZM33602EVM and LMZM33603EVM evaluation modules and TI's WEBENCH® Power Designer. Target applications for the LMZM3360x power modules include factory and building automation, smart grid and energy, industrial, medical, defense, and inverted output applications.

To learn more, visit www.mouser.com/ti-lmzm33602-lmzm33603-power-module.


With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room