Arduino MKR WAN 1300 and MKR GSM 1400, Now at Mouser Electronics, Offer Low-Power Connectivity for IoT Edge Devices
April 2, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MKR WAN 1300 and MKR GSM 1400 from Arduino.
The Arduino MKR WAN 1300 and MKR GSM 1400 boards are designed to offer a practical and cost-effective solution for developers, makers and enterprises, enabling them to quickly add connectivity to their projects and ease the development of battery-powered Internet of Things (IoT) edge applications. Offering 32-bit computational power similar to the Arduino MKR ZERO board, both the MKR WAN 1300 board and MKR GSM 1400 board are based on a Microchip SAM D21 microcontroller, which integrates an Arm Cortex-M0+ processor, 256 Kbytes of flash, and 32 Kbytes of SRAM.
The MKR WAN 1300 board adds LoRa connectivity through a Murata CMWX1ZZABZ Lo-Ra module and can be powered using two 1.5V AA or AAA batteries, or from an external 5V supply. The MKR GSM 1400 board adds a GSM module for global 3G communication and provides a rich set of Input and output (IO) interfaces, including eight digital IOs; 12 PWM outputs; UART, SPI and I2C interfaces; analog IO including seven inputs and one output; and eight external interrupt pins.
Both of the highly compact boards measure just 67.64 x 25.00 mm and offer low power consumption, making them an ideal choice for emerging battery-powered IoT edge devices in the MKR form factor for applications such as environmental monitoring, tracking, agriculture, energy monitoring and home automation.
To learn more about the MKR WAN 1300 board, go to www.mouser.com/arduino-mkr-wan-1300. For more information about the MKR GSM 1400 board, visit www.mouser.com/arduino-mkr-gsm-1400.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 22 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Arduino
Arduino is an open-source electronics prototyping platforms based on flexible, easy-to-use hardware and software. Arduino prototyping platforms are intended for artists, designers, beginners, hobbyists, and anyone interested in creating interactive objects or environments. Arduino projects can sense the environment by receiving input from a variety of sensors and can affect their surroundings by controlling lights, motors, and other actuators. Arduino projects can be stand-alone or they can communicate with software running on a computer.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com