Industry's Lowest Power 3.3V PCIe Clock Generators from IDT Now Shipping from Mouser
July 8, 2015 - Mouser Electronics, Inc. is now shipping the 9FGL PCI Express (PCIe) Clock Generators from Integrated Device Technology (IDT). The 9FGL family of clock generators are members of IDT's 3.3V low-power PCIe series and support both Common Clock (CC) with or without spread spectrum and Separate Reference no-Spread (SRnS) PCIe clocking architectures. Operating at 120mW and 130mW power consumption respectively, the 9FGL06 and 9FGL08 generators are the lowest power 3.3V PCIe clock generators available, eliminating thermal concerns in high-performance consumer devices.
The IDT 9FGL PCIe Clock Generators, available from Mouser Electronics, are low-power clock generators that generate low-power HCSL differential clock outputs in either 6-output (9FGL06) or 8-output (9FGL08) forms. All 9FGL clock generators feature support for two different spread spectrum levels plus an off function (0% spread). Direct connections to transmission lines and small 40-pin, 5mm x 5mm (9DFGL06) or 48-pin, 6mm x 6mm (9FGL08) VFQFPN packages reduce required board space and BOM costs. The 9FGL0641 and 9FGL0651 devices contain default configuration, and the 9FGL06P1 and 9FGL08P1 devices can be programmed with a user-defined power up default SMBus configuration. These SMBus-selectable features allow optimization options including control input polarity, control input pull up/downs, slew rate for each output, differential output amplitude, 33‑, 85‑, or 100‑ohm output impedance for each output, and spread spectrum amount.
Applications for the 9FGL family include computing systems, networking systems, industrial applications, and data-communications applications.
To learn more about the IDT 9FGL PCIe Clock Generators, visit
http://www.mouser.com/new/idt/idt-9fgl-generators/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Integrated Device Technology (IDT)
Integrated Device Technology, Inc. delivers system-level innovations that optimize customers' applications and enrich the end-user experience. IDT continues to build on its No. 1 positions in timing, serial switching and memory interfaces to expand its mixed-signal content in Communications, Computing and Consumer applications, driven by three major market drivers including cloud computing, consumer mobility and 4G/LTE. The company's product portfolio has become a fusion of analog and system expertise as well as traditional digital competencies, providing customers with complete application-optimized mixed-signal solutions. The IDT 30+ year heritage and innovation in digital technologies, coupled with its in-house analog talents and capabilities, make IDT the premier analog and digital company.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com